お客様の素早い設計とより早い製品化を実現する、技術情報と専門知識をご紹介します。
The JN517x-XK040 expansion kit contains components that can be used to form a ZigBee node based on the NXP JN5179 wireless microcontroller. The node provides lighting and sensor functionality. It can participate in a wireless network which may, for example, be created using components of the JN517x-DK005 or JN516x-EK004 kit. It can be introduced into the network via network commissioning or, optionally, via NFC commissioning using the NFC antenna on the supplied carrier board. The node supports the ZigBee 3.0 wireless networking protocol.
Pre-programmed software: The JN5179 module supplied in this kit is pre-programmed as a Dimmable Light for use in the ZigBee Smart Home Demonstration provided in the JN517x-DK005 Development Kit.
Re-programming: The JN5179 module can be re-programmed via a serial connection from a PC running a JN51xx Flash Programmer utility to download a new application to the Flash memory on the JN5179 device. A suitable utility is the JN51xx Production Flash Programmer (JN-SW-4107).
セクションを選択: