vsi v4l2 system structure definition

1. Standard v4l2 skeleton

										|- video device 0
										|
										|- video device 1
                    |
		v4l2-device	---	|...
			              |
										|- video device n

	1.1 v4l2 device
		v4l2 device is initialized by v4l2_device_register(). It has a 
	parent struct device *dev which is created from platform_device_register().
		Commonly v4l2 device is embedded in a larger structure as global control.
	We can refer to struct vsi_v4l2_device for example.
	
	1.2 video device
		Each video device is created by video_device_alloc() and registered to system
	by video_register_device().
		It is connected to v4l2 device as its parent device. Each video device has a 
	file in	/dev/ according to its capability. E.g. for video device it is
	/dev/video*. So each video device has open/close/read/write/ioctl/mmap/poll
	interfaces as standard files do.
	
	1.3 ioctls
		Each video device's ioctl will go through v4l2's kernel standard ioctl
	API. They will finally call video device's ioctl_ops callbacks. Ioctl callbacks
	are set through struct v4l2_ioctl_ops as a member	of video device. 
	vsi_v4l2_ioctl is our realization of it. Most of our member functions use
	default value since it's easier to comply to v4l2 standard this way.
	
	1.4 controls
		v4l2's controls is used to configure video device operation parameters. There
	are	three kinds of controls: standard, standard menu (where there's a range of
	choice) and custom defined control. Each custom control has a standard structure
	to define its content. Each control must have a structure v4l2_ctrl_ops	for
	v4l2 callback to set/get. I write vsi_setup_ctrls() as example, it sets up one
	control	for each kind of control.
	
	1.5 v4l2 file handle
	For each open operation of v4l2 video device which go through open API, v4l2 will
	register it with v4l2_fh_init() and v4l2_fh_add(). We just use it to store some
	private data now. Currently we create context for each opened file handle.
	
	1.6 v4l2 subdev
	Another important part of v4l2 is subdev. We don't use it in current stage and
	will update its information later.
	
	1.7 v4l2 queue management: vb2_queue and vb2_buffer
	The critical functionality of v4l2 is buffer control, which is realized through
	v4l2 queue management. Each video device manages one or more structure vb2_queue.
	Each vb2_queue manages a number of struct vb2_buffer as their content. 
	vb2_buffer has internal structure to represent a buffer, who may have over one
	planes. How to organize and use these buffers are determined by system
	requirement and driver realization. In most cases we've saw they are link as a list.
	
	struct vb2_queue_init has rich parameters. It is initialized by vb2_queue_init().
	There're two groups of important callbacks: ops and mem_ops. Another group of
	callbacks is vb2_buf_ops, which is rarely used and whose meaning is not clear.
	
	1.7.1 mem_ops callbacks of vb2_queue
	mem_ops is used as alloc, free, mmap, ref/unref, transfer logic address, 
	attach/detach dmabuf, etc. These callbacks are used internally by v4l2 kernel,
	thus they won't be called explicitly. Kernel provides two well defined
	realization: vb2_dma_contig_memops and vb2_vmalloc_memops. Almost all
	v4l2 drivers use either of them. We use vb2_dma_contig_memops since we're
	familiar with DMA_BUF operation.
	
	1.7.2 ops callbacks of vb2_queue
	ops is used as callbacks when v4l2 kernel need do something on buffer in
	certain operation. Most of these callbacks don't have default value. How to
	realize these callbacks depends on v4l2's requirement of them and how
	our v4l2 driver manages buffers. This is critical.
	There're three kind of buffer, which is transferred as parameter in
	VIDIOC_REQBUFS: V4L2_MEMORY_DMABUF, V4L2_MEMORY_MMAP, V4L2_MEMORY_USERPTR.
	Actually there's fourth kind: V4L2_MEMORY_OVERLAY, which is very rarely
	used. V4L2_MEMORY_DMABUF means all buffers are DMA_BUF allocated by
	caller app and shared through DMA_BUF's file handle. V4L2_MEMORY_USERPTR
	means input buffer are allocated by user app and shared by mem mapping
	user pointer. V4L2_MEMORY_MMAP means v4l2 driver should allocate buffer
	by itself and returned them to user space app. We'll support only
	V4L2_MEMORY_MMAP according to our hardware's limit and software
	flexibility.
	
	1.7.3 simple example of queue usage in v4l2 application
	A simple application using v4l2 to codec looks like this:
	Through VIDIOC_REQBUFS ioctl, buffer type and number are determined.
	Then user space app will use VIDIOC_QBUF on each buffer to add them
	to v4l2 driver's queue. Then VIDIOC_STREAMON is called. Application
	will wait for VIDIOC_DQBUF for ready buffer returned from v4l2 driver.
	Note that returned buffer in VIDIOC_DQBUF might not be identical to
	its input, since which buffer is ready is decided by v4l2 driver.
	After returned buffer is used up, it can be VIDIOC_QBUF to v4l2
	driver to use again.
	
2. Spec and Test package for v4l2

	v4l2 has spec for user space app, which is attached in wiki as v4l2.pdf.
	v4l2 kernel driver does not have spec. Currently there're two
	sets of utils to test single API of kernel driver:
	v4l-utils: a set of v4l utils. It's a part of apt-get project.
	linux test project: git https://github.com/linux-test-project/ltp.git.
		It has a sub directory for v4l2.
	
3. VSI v4l2 driver structure
	
	Currently VSI v4l2 driver uses stateful method to haste coding
	and reduce porting problem. Whole system looks like this:
	
	
			v4l2 user space app										VSI v4l2 user space daemon
			(ffmpeg, gst, etc.)								/
																			/									|
					|		|											/										|
					|		|ioctls							/	msg pipe					VSI middle ware
					|		|									/		for msg							|
					|		|								/			exchange						|
					|		|							/														|
	
		VSI v4l2 kernel driver											VSI codec kernel driver
	
	3.1 v4l2 user space app
	v4l2 user space app is conformant to v4l2 user space spec. It needs
	only communicate with VSI v4l2 kernel driver by ioctls and other
	standard file operations. It can't see VSI v4l2 user space daemon,
	nor VSI middle ware, nor VSI codec kernel driver.
	
	3.2 VSI v4l2 kernel driver
	VSI v4l2 kernel driver should be conformant to v4l2 kernel driver
	definition.	It has three main functionalities.
	3.2.1
		Link v4l2 user space app with VSI v4l2 daemon. It receives command from
		v4l2 user space app by ioctl, reformat it, write it to VSI v4l2
		daemon through message pipe, receives return value from VSI daemon
		through message pipe and returns it to v4l2 user space app. Currently
		message pipe is realized through standard file read/write API.
	3.2.2
		Manage buffers, including buffer allocation, buffer sharing and queue
		control.
	3.2.3
		Internal state maintaining. This is used to reduce message exchange
		with VSI v4l2 daemon.
	
	3.3 VSI v4l2 kernel driver device files
		To realize functionality in 3.2 VSI v4l2 driver creates two device files:
		/dev/video*, file for v4l2 user space app to use.
		/dev/v4l2,   file for message exchange with VSI v4l2 daemon.
		
	3.4 VSI v4l2 user space daemon
		This daemon has two aspects: it exchange command and state with v4l2
		kernel driver through message pipe; it controls VSI codec through
		middle ware.
		
4. VSI v4l2 Code organization	(may change in future)
	<project.v4l2>
        +-- develop (developing branch)
                  +-- doc
                  +-- v4l2_vsi_daemon (user space)
                  |     
                  +-- v4l2_vsi_driver
                  |        +-- vsi_v4l2.c				v4l2 kernel driver skeleton
                  |        +-- v4l2-daemon.c		message pipe management
                  |
                  +-- test
                           +-- unit (unit test for some function)
                           +-- ffmpeg (testing the integrate to ffmpeg)
                           +-- gst (testing the integrate to ffmpeg)
                           +-- comform (conformance testing)