Metadata-Version: 2.1
Name: littlefs-python
Version: 0.3.0
Summary: A python wrapper for littlefs
Home-page: https://github.com/jrast/littlefs-python
Author: Jürg Rast
Author-email: juergr@gmail.com
License: UNKNOWN
Platform: UNKNOWN
Classifier: Development Status :: 3 - Alpha
Classifier: Intended Audience :: Developers
Classifier: Programming Language :: Python :: 3
Classifier: Topic :: Scientific/Engineering
Classifier: Topic :: Software Development :: Embedded Systems
Classifier: Topic :: Software Development :: Libraries
Classifier: Topic :: System :: Filesystems
Description-Content-Type: text/x-rst
License-File: LICENSE

===================
littlefs for Python
===================

.. image:: https://travis-ci.org/jrast/littlefs-python.svg?branch=master
    :target: https://travis-ci.org/jrast/littlefs-python
    :alt: Build Status: Linux

.. image:: https://ci.appveyor.com/api/projects/status/v7i08nhfbs2e0vro?svg=true
    :target: https://ci.appveyor.com/project/jrast/littlefs-python
    :alt: Build Status: Windows

.. image:: https://readthedocs.org/projects/littlefs-python/badge/?version=latest
    :target: https://littlefs-python.readthedocs.io/en/latest/?badge=latest
    :alt: Documentation Status

.. image:: https://badge.fury.io/py/littlefs-python.svg
    :target: https://badge.fury.io/py/littlefs-python

littlefs-python provides a thin wrapper around littlefs_, a filesystem targeted for
small embedded systems.
The wrapper provides a pythonic interface to the filesystem and allows the creation,
inspection and modification of the filesystem or individual files.
Even if this package uses Cython_, the goal is not to provide a high performance
implementation. Cython was chosen as an easy method is offered to generate the binding
and the littlefs library in one step.

Quick Examples
==============
Let's create a image ready to transfer to a flash memory using the pythonic interface:

.. code:: python

    from littlefs import LittleFS

    # Initialize the File System according to your specifications
    fs = LittleFS(block_size=512, block_count=256)

    # Open a file and write some content
    with fs.open('first-file.txt', 'w') as fh:
        fh.write('Some text to begin with\n')

    # Dump the filesystem content to a file
    with open('FlashMemory.bin', 'wb') as fh:
        fh.write(fs.context.buffer)

The same can be done by using the more verbose C-Style API, which closely resembles the
steps which must be performed in C:

.. code:: python

    from littlefs import lfs

    cfg = lfs.LFSConfig(block_size=512, block_count=256)
    fs = lfs.LFSFilesystem()

    # Format and mount the filesystem
    lfs.format(fs, cfg)
    lfs.mount(fs, cfg)

    # Open a file and write some content
    fh = lfs.file_open(fs, 'first-file.txt', 'w') as fh:
    lfs.file_write(fs, fh, b'Some text to begin with\n')
    lfs.file_close(fs, fh)

    # Dump the filesystem content to a file
    with open('FlashMemory.bin', 'wb') as fh:
        fh.write(cfg.user_context.buffer)


Installation
============

This is as simple as it can be::

    pip install littlefs-python

At the moment wheels (which require no build) are provided for the following platforms,
on other platforms the source package is used and a compiler is required:

 - Linux: Python 3.6 - 3.10 / 32- & 64-bit
 - Windows: Python 3.6 - 3.10 / 32- & 64-bit


Development Setup
=================

Start by checking out the source repository of littlefs-python::

    git clone https://github.com/jrast/littlefs-python.git

The source code for littlefs is included as a submodule which must be
checked out after the clone::

    cd <littlefs-python>
    git submodule update --init

this ensures that the correct version of littlefs_ is cloned into
the littlefs folder. As a next step install the dependencies and install
the package::

    pip install -r requirements.txt
    pip install -e .

.. note::
    It's highly recommended to install the package in a virtual environment!


Development Hints
-----------------

- Test should be run before commiting: `pytest test`
- Mypy is used for typechecking. Run it also on the tests to catch more issues:
  `mypy src test test/lfs`
- Mypy stubs can be generated with `stubgen src`. This will create a `out` direcotry
  containing the generated stub files.


Creating a new release
======================

- Make sure the master branch is in the state you want it.
- Create a tag with the new version number
- Wait until all builds are completed. A new release should be created
  automatically on github.
- Build the source distribution with `python setup.py sdist`
- Download all assets (using `ci/download_release_files.py`)
- Upload to pypi using twine: `twine upload dist/*`



.. _littlefs: https://github.com/littlefs-project/littlefs
.. _Cython: http://docs.cython.org/en/latest/index.html