Overview
========
The CRC Example project is a demonstration program that uses the KSDK software to generate checksums
for an ASCII string. Several CRC protocols are implemented using the CRC driver API.


Toolchain supported
===================
- IAR embedded Workbench 7.50.1
- Keil MDK 5.17
- GCC ARM Embedded 2015-4.9-q3
- Kinetis Development Studio IDE 3.0.0
- Atollic TrueSTUDIO 5.4.0

Hardware requirements
=====================
- Mini/micro USB cable
- FRDM-KL27Z board
- Personal Computer

Board settings
==============
This example project does not call for any special hardware configurations.
Although not required, the recommendation is to leave the development board's jumper settings
and configurations in default state when running this example.

Prepare the Demo
================
Connect a serial cable from the debug UART port of the board to the PC. Start Tera Term
(http://ttssh2.osdn.jp) and make a connection to the virtual serial port.

1. Start Tera Term
2. New connection -> Serial
3. Set apropriate COMx port (x is port number) in Port context menu. Number is provided by operation
   system and could be different from computer to computer. Select COM number related to virtual
   serial port. Confirm selected port by OK button.
4. Set following connection parameters in menu Setup->Serial port...
        Baud rate:    115200
        Data:         8
        Parity:       none
        Stop:         1
        Flow control: one
5.  Confirm selected parameters by OK button.


Running the demo
================
Example output on terminal:

CRC Peripheral Driver Example

Test string: 123456789
CRC-16 CCIT FALSE: 0x29b1
CRC-16 MAXIM: 0x44c2
CRC-16 KERMIT: 0x2189
CRC-32: 0xcbf43926
CRC-32 POSIX: 0x765e7680

Customization options
=====================