Overview
========
The TPM project is a simple demonstration program of the SDK TPM driver. It sets up the TPM
hardware block to output PWM signals on two TPM channels. The PWM dutycycle on both channels
is periodically updated. On boards that have an LED connected to the TPM pins, the user will see
a change in LED brightness.

Toolchain supported
===================
- IAR embedded Workbench 7.50.1
- Keil MDK 5.17
- GCC ARM Embedded 2015-4.9-q3
- Kinetis Development Studio IDE 3.0.0
- Atollic TrueSTUDIO 5.4.0

Hardware requirements
=====================
- Mini/micro USB cable
- FRDM-K27Z board
- Personal Computer

Board settings
==============
This MPU Example project does not call for any special hardware configurations.
Although not required, the recommendation is to leave the development board's jumper settings
and configurations in default state when running this example.

Prepare the Demo
================
1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.
2. Open a serial terminal with these settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo
================
When the example runs successfully, you can see information from the terminal as below.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
TPM example to output PWM on 2 channels
You will see a change in LED brightness if an LED is connected to the TPM pin
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

Customization options
=====================