Overview
========
This document explains the freertos_sem example, what to expect when running it and a brief
introduction to the API. The freertos_sem example code shows how semaphores works. Two different
tasks are synchronized in bilateral rendezvous model.

The example uses four tasks. One producer_task and three consumer_tasks. The producer_task starts by
creating of two semaphores (xSemaphore_producer and xSemaphore_consumer). These semaphores control
access to virtual item. The synchronization is based on bilateral rendezvous pattern. Both of
consumer and producer must be prepared to enable transaction.


Toolchain supported
===================
- IAR embedded Workbench 7.50.1
- Keil MDK 5.17
- GCC ARM Embedded 2015-4.9-q3
- Kinetis Development Studio IDE 3.0.0
- Atollic TrueSTUDIO 5.4.0

Hardware requirements
=====================
- Mini/micro USB cable
- FRDM-KL27Z board
- Personal Computer

Board settings
==============
This example project does not call for any special hardware configurations.
Although not required, the recommendation is to leave the development board's jumper settings
and configurations in default state when running this example.

Prepare the Demo
================
Connect a serial cable from the debug UART port of the board to the PC. Start Tera Term
(http://ttssh2.osdn.jp) and make a connection to the virtual serial port.

1. Start Tera Term
2. New connection -> Serial
3. Set apropriate COMx port (x is port number) in Port context menu. Number is provided by operation
   system and could be different from computer to computer. Select COM number related to virtual
   serial port. Confirm selected port by OK button.
4. Set following connection parameters in menu Setup->Serial port...
        Baud rate:    115200
        Data:         8
        Parity:       none
        Stop:         1
        Flow control: one
5.  Confirm selected parameters by OK button.



Running the demo
================
After the board is flashed the Tera Term will show debug console output.

Example output:
Producer_task created.
Consumer_task 0 created.
Consumer_task 1 created.
Consumer_task 2 created.
Consumer number: 0
Consumer 0 accepted item.
Consumer number: 1
Consumer number: 2
Producer released item.
Consumer 0 accepted item.
Producer released item.
Consumer 1 accepted item.
Producer released item.
Consumer 2 accepted item.

Customization options
=====================