Overview
========
The LPUART example for FreeRTOS demonstrates the possibility to use the LPUART driver in the RTOS.
The example uses single instance of LPUART IP and writes string into, then reads back chars.
After every 4B received, these are sent back on LPUART.

Toolchain supported
===================
- IAR embedded Workbench 7.50.1
- Keil MDK 5.17
- GCC ARM Embedded 2015-4.9-q3
- Kinetis Development Studio IDE 3.0.0
- Atollic TrueSTUDIO 5.4.0

Hardware requirements
=====================
- Mini USB cable
- FRDM-KL43Z board
- Personal Computer

Board settings
==============
No special is needed.

Prepare the Demo
================
1.  Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
2.  Open a serial terminal on PC for OpenSDA serial device with these settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Reset the SoC and run the project.

Running the demo
================
You will see the welcome string printed out on the console.
You can send characters to the console back and they will be printed out onto console in a group of 4 characters.

Customization options
=====================