Overview
========

The cmt example shows the simplest way to use CMT driver.

In this example, the CMT is work as Time mode and used to modulation 11 bit numbers of data.
The CMT is configured to generate a 40000hz carrier generator signal through a modulator gate
configured with different mark/space time period to represent bit 1 and bit 0. 
The modulated data rate is 9600.

Note, The end of cycle interrupt provides a means for the user to reload new mark/space values
into the modulator data registers. Modulator data register updates will take effect at the end 
of the current modulation cycle. The CMT internal down-counter and space period register are
updated at the end of every modulation cycle, irrespective of interrupt handling and the state
of the interrupt. so please make sure the IRQ handler process is shorter than the modulation
cycle to ensure the new mark/space counter is prepared before each end of modulation cycle.

Toolchain supported
===================
- IAR embedded Workbench 7.50.1
- Keil MDK 5.17
- GCC ARM Embedded 2015-4.9-q3
- Kinetis Development Studio IDE 3.0.0
- Atollic TrueSTUDIO 5.4.0

Hardware requirements
=====================
- Mini/micro USB cable
- TWR-K80F150M board
- Personal Computer
- Osciloscope

Board settings
==============
This CMT Example project does not call for any special hardware configurations.
Although not required, the recommendation is to leave the development board's jumper settings
and configurations in default state when running this example.
Osciloscope needs configuring to easily capture the signal:
    - Trigger should be used to capture the output signal.
    - Set the voltage range to 1 voltage, and adjust the scale to make the smallest time unit to about 400 us.

Prepare the Demo
================
1.  Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
2.  Open a serial terminal on PC for OpenSDA serial device with these settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Connect a oscilloscope the pin 1 of the Jumper 15 on TWR-K80F150M.
4.  Download the program to the target board.
5.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
When the demo runs, the log would be seen on the OpenSDA terminal like:
~~~~~~~~~~~~~~~~~~~~~~~~~~~
CMT Example Start.
CMT DATA Modulate Finished.
CMT Example End.
~~~~~~~~~~~~~~~~~~~~~~~~~~~
Note
The example modulates 11 bit data is modulated and output as: 10001100011.
The output waveform is captured on the oscilloscope like:
    - data order: 1 -> 0 -> 0 -> 0 -> 1 -> 1 -> 0 -> 0 -> 0 -> 1 -> 1
    - the period of the basic carrier generator signal is 25 microsecond
    - bit 1 is about four normal carrier signal period.
    - bit 0 is about one normal carrier signal period and three space carrier signal period.

Customization options
=====================