Overview
========
The i2c_read_accel_value example shows how to use I2C driver to communicate with an i2c device:

 1. How to use the i2c driver to read a i2c device who_am_I register.
 2. How to use the i2c driver to write/read the device registers.

In this example, the values of three-axis accelerometer print to the serial terminal on PC through
the virtual serial port on board.

Toolchain supported
===================
- IAR embedded Workbench 7.50.1
- Keil MDK 5.17
- GCC ARM Embedded 2015-4.9-q3
- Kinetis Development Studio IDE 3.0.0
- Atollic TrueSTUDIO 5.4.0

Hardware requirements
=====================
- Mini/Micro USB cable
- TWR-K80F150M board
- Personal Computer

Board settings
==============
No special is needed.

Prepare the Demo
================
1.  Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
2.  Open a serial terminal on PC for OpenSDA serial device with these settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
When the example runs successfully, you can see the similar information from the terminal as below.
I2C example -- Read Accelerometer Value
Found a MMA8451 on board , the device address is 0x1d .
The accel values:
status_reg = 0xff , x =   -10 , y =    31 , z =  2025
status_reg = 0xff , x =    -6 , y =    32 , z =  2022
status_reg = 0xff , x =    -9 , y =    35 , z =  2023
status_reg = 0xff , x =    -4 , y =    32 , z =  2034
status_reg = 0xff , x =   -12 , y =    32 , z =  2020
status_reg = 0xff , x =    -8 , y =    33 , z =  2022
status_reg = 0xff , x =    -8 , y =    33 , z =  2017
status_reg = 0xff , x =    -9 , y =    35 , z =  2024
status_reg = 0xff , x =    -7 , y =    35 , z =  2018
status_reg = 0xff , x =    -5 , y =    33 , z =  2019
End of I2C example .

Customization options
=====================