Overview
========
The pee_bple example shows how to use MCG driver to change from PEE mode to BLPE mode:

 1. How to use the mode functions for MCG mode switch.
 2. How to use the frequency functions to get current MCG frequency.
 3. Work flow
    Boot to PEE mode from default reset mode
    Change mode PEE -> PBE -> BLPE
    Change back BLPE -> PBE -> PEE
    Get System clock in PEE mode to blink LED

In this example, because the debug console's clock frequency may change,
so the example running information is not output from debug console. Here the
LED blinks to show that the example finished successfully.

Toolchain supported
===================
- IAR embedded Workbench 7.50.1
- Keil MDK 5.17
- GCC ARM Embedded 2015-4.9-q3
- Kinetis Development Studio IDE 3.0.0
- Atollic TrueSTUDIO 5.4.0

Hardware requirements
=====================
- Mini/Micro USB cable
- TWRK80F150M board
- Personal Computer

Board settings
==============
No special board settings.

Prepare the Demo
================
1. Connect a mini/micro USB cable between the PC host and the OpenSDA USB port on TWRK80F150M board.
2. Download the program to the target board.
3. Either press the reset button on your board or launch the debugger in your IDE to begin running
   the demo. For detailed instructions, see Getting Started with Software Development Kit for
   K80F150M.

Running the demo
================
When the demo runs successfully, the board's LED will blink.

Customization options
=====================