#!/bin/bash # # Copyright 2017-2019 NXP # # SPDX-License-Identifier: BSD-3-Clause # # A general distro installer with flexibly configurable partitions and fully available capacity # of target disk during installing, which overcomes the disadvantage that users have to resize # the remaining unformatted space of target disk when using the way of "dd" or "wic". # # Author: Shengzhou Liu # set -e FIVERSION=1.12.2012 DEFAULT_DISK_PARTITION="4P=128M:2G:5G:-1" DEFAULT_LOOP_DEVICE_PARTITION="4P=128M:2G:64M:-1" DEFAULT_SDCARD_IMG_SIZE_MB=5120 DEFAULT_RAW_PARTITION_SIZE_MB=64 DEFAULT_DISTRO_SVR_URL=http://www.nxp.com/lgfiles/sdk/lsdk2012 usage () { cat < ] [ -b ] [ -r ] [ -f ] [ -d ] [ -m ] OPTION: -i, --instruction Instruction to execute, valid argument as below: 'auto' Automatically partition and format the target storage drive, then download and install distro images 'pf' Only partition and format the target storage drive without installing distro images 'download' Only download distro images without installation 'install' Only install the specified image, can be omitted by default 'list' Show the list of supported machines and installation invironment 'backup' Backup rootfs and bootpartition as tarball 'mksdcard' Create sdcard.img including composite firmware and distro images -b, --bootimg The boot partition image -r, --rootfsimg The root partition image -B, --bootpart Specify boot partition number to override default (default boot partition is the 2nd) -R, --rootpart Specify root partition number to override default (default root partition is the last) -d, --device Device name of the target SD/USB/SATA storage drive in Linux -p, --partition Customize configurable partitions of target disk, default is "-p 4P=100M:2G:5G:-1" if not specified -f, --firmware The composite firmware image to be programmed into SD card (only for SD boot) -F, --force Force partition and format target disk regardless of the existing data in disk -e, --efi Used for the case of UEFI as bootloader instead of U-Boot, valid argument: dtb or acpi -m, --machine Target machine name to specify the name of composite firmware for automatical deployment -u, --url Specify URL of distro webserver to override the default one for automatically downloading distro -v, --version Print version info -h, --help Print help info Examples for various use scenarios: - Automatically download and install LSDK distro images to target storage drive on host machine or ARM board: $ flex-installer -i auto -m ls1046ardb -d /dev/mmcblk0 (automatically install the latest LSDK distro) You can specify one or several of '-b -r -f -u ' options to override the default settings - To partition and format target SD/eMMC/USB disk and install custom distro image: $ flex-installer -i pf -d /dev/mmcblk0 (default 4 partitions as 4P=128M:2G:5G:-1) or $ flex-installer -i pf -d /dev/sdx -p 4P=128M:3G:6G:-1 (specify custom partitions as 4P=128M:3G:6G:-1) $ flex-installer -b boot_arm64_lts_5.4.tgz -r rootfs_ubuntu_arm64.tgz -f firmware__sdboot.img -d /dev/sdx (install multiple images) or $ flex-installer -r rootfs_ubuntu_main_arm64.tgz -d /dev/sdx (only install root partition image) $ flex-installer -b boot_arm64_lts_5.4.tgz -d /dev/sdx (only install boot partition image) $ flex-installer -f firmware__sdboot.img -d /dev/sdx (only install composite firmware image) - Install local distro image with custom 3 partitions, to specify partition-1 for boot partition and partition-3 for rootfs partition: $ flex-installer -i pf -p 3P=2G:4G:-1 -d /dev/mmcblk0 $ flex-installer -b -r -f -d /dev/mmcblk0 --bootpart=1 --rootpart=3 After installing successfully, run "setenv devpart_boot 1;setenv devpart_root 3;boot" in U-Boot to boot distro from the specific partition) - On ARM board in TinyLinux environment, firstly partition target disk, then download distro images onto board and install as below: 1. flex-installer -i pf -d /dev/mmcblk0 (or /dev/sdx) 2. cd /mnt/mmcblk0p4 (or /mnt/sdx4) and download distro images to this partition via wget or scp 3. flex-installer -r -b -f -d /dev/mmcblk0 (or /dev/sdx) - Convert distro tarball images into sdcard.img in configurable scheme of partitions $ flex-installer -i mksdcard -p 3P=1G:1G:-1 -r -f [ -b ] - Backup rootfs and bootpartition from target storage device $ flex-installer -i backup -d /dev/sdx Note: '-e dtb' or '-e acpi' option is needed if UEFI is used as bootloader, no need in case of U-Boot. EOF exit } search_dev() { devlist=`ls /dev/sd?` for dev in $devlist; do sdx=`udevadm info -q all -n $dev | grep ID_BUS` disksize=$[ `sudo fdisk -ls $dev` / 1000000 ] if [ $1 = usb ] ; then if [ ${sdx:10:3} = usb ]; then devusb=${dev:5:3} echo "USB disk: $devusb $disksize GB" break fi elif [ $1 = sata ]; then if [ ${sdx:10:3} = ata ]; then devsata=${dev:5:3} echo "SATA disk: $devsata $disksize GB" break fi fi done } get_device_name_in_tinydistro() { # for automation test with '-d sd|usb|sata' instead of '-d /dev/sdx' in tiny distro by searching 1st available device on remote board if [ "$mediadevice" = "sd" ]; then [ ! -b /dev/mmcblk0 ] && echo "SD/MMC device is not available" && exit || devname=mmcblk0 elif [ "$mediadevice" = "usb" ] ; then search_dev usb devname=$devusb [ -z "$devname" ] && echo "USB device is not available" && exit elif [ "$mediadevice" = "sata" ] ; then search_dev sata devname=$devsata [ -z "$devname" ] && echo "SATA device is not available" && exit elif echo "$mediadevice" | grep -q /; then devname=${mediadevice##*/} fi [ ${devname:0:6} = mmcblk -o ${devname:0:4} = loop ] && devpartname=${devname}p || devpartname=$devname } get_device_name_on_host() { devname=${mediadevice##*/} [ ${devname:0:6} = mmcblk -o ${devname:0:4} = loop ] && devpartname=${devname}p || devpartname=$devname } umount_device() { mntlist=$(cat /proc/mounts | grep /dev/${devpartname} | cut -d' ' -f1 | tr '\n' ' ') for mntp in $mntlist; do if [ $intinyrfs = y -a `pwd` = $rootpartition ]; then continue else sudo fuser -k $mntp || true sudo umount $mntp || true fi done } mount_device() { [ $pnum -ge 5 ] && max=$[ $pnum + 1 ] || max=$pnum for i in $(seq 1 $max); do [ $pnum -ge 5 -a $i = 4 ] && continue sudo mkdir -p $mntdir/${devpartname}$i if ! mount | grep -q ${devpartname}$i; then sudo mount /dev/${devpartname}$i $mntdir/${devpartname}$i 1>/dev/null 2>&1 || true fi done } program_firmware_to_sd() { # $1: firmware file, $2: startblock, $3: device [ ! -b $3 ] && echo device $device not found && exit [ ! -r $1 ] && echo firmware $1 not found && exit sudo dd if=$1 of=$3 bs=512 seek=$2 print_d "Program $1 into $3 startblock=$2" } check_partition_number() { [ -z "$diskpartition" ] && print_e "Please specify partition settings" && exit if ! [[ $diskpartition =~ ^[2-9]+[P=]+[0-9]+[G,M]* ]] || \ echo $diskpartition | tr -d '[0-9] [:,-]' | grep -E '[^P,M,G]'; then print_e "Error: the number of partitions should be >= 2 and the unit of size is G or M" print_w "Correct example: '-p 5P=100M:2G:5G:6G:-1', '-1' indicates the rest space of target disk for the last partition as rootfs" exit fi pnum=`echo $diskpartition | cut -d= -f1` pnum=${pnum%?} partlistnum=$(echo $diskpartition | awk -F":" '{print NF-1}') partlistnum=$[ $partlistnum + 1 ] [ $pnum != $partlistnum ] && print_e "ERROR: You set $pnum partitions, but listed $partlistnum partitions" && exit || true [ $pnum -ge 5 ] && totalparts=$[ $pnum + 1 ] || totalparts=$pnum } check_device_partitions() { [ -n "$firmware" -a -z "$bootimg" -a -z "$rootfsimg" ] && return [ -b /dev/$devname ] || { print_w "/dev/$devname not found"; exit; } [ -n "$diskpartlist" ] && partition_format_disk $diskpartition && return if sudo parted -s /dev/$devname print 2>/dev/null | grep -qE 'unrecognised disk|Partition Table: unknown'; then partition_format_disk $diskpartition && return fi pnum=$(sudo parted -s /dev/$devname print | grep -E "^ [0-9]" | wc -l) if sudo parted -s /dev/$devname print | grep -q extended; then pnum=$[ $pnum -1 ]; fi [ $pnum -le 4 ] && rootpartnum=$pnum || rootpartnum=$[ $pnum + 1 ] backuppartnum=$[ $rootpartnum - 1 ] rootpartition=$mntdir/${devpartname}${rootpartnum} && rootdev=/dev/${devpartname}$rootpartnum backuppartition=$mntdir/${devpartname}${backuppartnum} && backupdev=/dev/${devpartname}$backuppartnum mount_device [ ! -f /mnt/${devpartname}$rootpartnum/etc/buildinfo -a -z "$rootfsimg" -a $instruction != auto ] && \ print_w "Not found valid rootfs installed on /dev/${devpartname}$rootpartnum, please specify '-r '" && exit true } partition_format_disk() { if mount | grep -q "$rootdev on / type"; then print_w "The target /dev/$devname can't be the running device in which $rootdev is running as rootfs" print_w "You can choose a non-running device or do the installation in TinyLinux environment" && exit fi print_n "Partitioning /dev/$devname ..." [ -z "$force_install" -a ${devname:0:4} != loop -a $instruction != pf ] && check_distro_in_disk optimal_io_size=$(sudo cat /sys/block/$devname/queue/optimal_io_size) minimum_io_size=$(sudo cat /sys/block/$devname/queue/minimum_io_size) [ "$optimal_io_size" = "0" ] && aligntype=minimal || aligntype=optimal [ $pnum -le 2 ] && parttable=gpt || parttable=msdos umount_device sudo rm -rf /mnt/${devpartname}*/* sudo parted -a $aligntype -s /dev/$devname mklabel $parttable for ((i=1; i<=$pnum; i++)); do eval n_p$i=`echo $1 | cut -d: -f$i` [ $i = 1 ] && n_p1=`echo $n_p1 | cut -d= -f2` n_p=`eval echo '${n_p'"$i"'}'` [ ${n_p: -1} = G ] && n_p=${n_p%?} && n_p=$[ $n_p * 1024 ] [ ${n_p: -1} = M ] && n_p=${n_p%?} [ ${n_p: -2} = -1 ] && eval e_p$i=100% [ $i = 1 ] && s_p1=$[ $DEFAULT_RAW_PARTITION_SIZE_MB + 4 ] && e_p1=$[ $s_p1 + $n_p ] && umount_device && \ sudo parted -a $aligntype -s /dev/$devname mkpart primary ${s_p1}MiB ${e_p1}MiB && continue n=$[ i-1 ] && a_e_p=`eval echo '${e_p'"$n"'}'` eval s_p$i=$[ $a_e_p + 1 ] && s_p=`eval echo '${s_p'"$i"'}'` [ ${n_p: -2} = -1 ] && eval e_p$i=100% || eval e_p$i=$[ $s_p + $n_p ] e_p=`eval echo '${e_p'"$i"'}'` if [ $pnum -le 4 ]; then parttype=primary elif [ $i -le 3 ]; then parttype=primary elif [ $i -eq 4 ]; then parttype=extended end=100% umount_device sudo parted -a $aligntype -s /dev/$devname mkpart $parttype ${s_p}MiB $end s_p=$[ $s_p + 1 ] parttype=logical extendedpart=4 else parttype=logical fi [ $e_p != 100% ] && end=${e_p}MiB || end=${e_p} umount_device sudo parted -a $aligntype -s /dev/$devname mkpart $parttype ${s_p}MiB $end done print_n "Formatting partitions ..." [ -f /usr/bin/man -a ${devname:0:4} != loop ] && man ext4 | grep -q metadata_csum && metadataopt=",^metadata_csum" for ((i=1; i<=$totalparts; i++)); do if [ $i = "$bootpartnum" ]; then umount_device sudo mkfs.ext4 -F -q -b 4096 -L boot -O ^64bit$metadataopt $bootdev || true elif [ $i = "$efipartnum" ]; then if [ "$enable_efi" = "y" ]; then # in case of UEFI as Bootloader umount_device sudo mkfs.vfat -n EFI $efidev || true else # for misc metadata or other uses in case of U-Boot as Bootloader umount_device sudo mkfs.ext4 -F -q -b 4096 -L misc $efidev || true fi else if [ $i = "$rootpartnum" ]; then label=system elif [ $i = "$backuppartnum" ]; then label=backup else label=data$i fi umount_device [ $i != "$extendedpart" ] && sudo mkfs.ext4 -F -q -O ^huge_file,^64bit$metadataopt -b 4096 -L $label /dev/${devpartname}$i || true fi done mount_device sudo parted -s /dev/$devname print print_d "partition and format /dev/$devname" } flex_install_distro() { # install composite firmware if [ -n "$firmware" -o $instruction = auto ] && [ -f $firmware_n ]; then umount_device program_firmware_to_sd $firmware_n 8 /dev/$devname fi mount_device # install boot partition if [ -n "$bootimg" -o $instruction = auto ] && [ -d $bootimg_n -o -f $bootimg_n ]; then [ -f $bootpartition/buildinfo ] && echo Cleaning the existing data in $bootdev && \ sudo rm -rf $bootpartition/* echo Installing $bootimg_n to $bootdev, waiting ... [ $bootimgtype = dir ] && sudo cp -rfp $bootimg_n/* $bootpartition [ $bootimgtype = tgz ] && sudo tar xf $bootimg_n -C $bootpartition print_d "Install $bootimg_n in $bootdev" fi # install system rootfs if [ -n "$rootfsimg" -o $instruction = auto ] && [ -d $rootfsimg_n -o -f $rootfsimg_n ]; then check_running_rfs $rootdev [ -d $rootpartition/var/lib ] && check_directory $rootpartition echo Installing $rootfsimg_n to $rootdev, waiting ... if mount | grep -q "$rootdev on / type"; then print_w "Can't install rootfs image to the running root filesystem" && exit fi case $rfsimgtype in dir) sudo cp -rfp $rootfsimg_n/* $rootpartition;; tgz) sudo tar xf $rootfsimg_n -C $rootpartition;; ext) dd if=$rootfsimg_n of=$rootdev bs=4M && sync;; cpio.gz) mv $rootfsimg_n $rootpartition && cd $rootpartition && \ gunzip $rootfsimg_n && cpio -idm < ${rootfsimg_n::-3} && cd -;; *) echo format $rfsimgtype is not supported; exit esac print_d "Install $rootfsimg_n in $rootdev" fi if [ $instruction = auto -o $instruction = install -o $instruction = null ]; then if [ $bootpartnum != 0 ]; then uuid_boot=$(lsblk -l --output UUID $bootdev | grep -) [ -z "$uuid_boot" ] && print_e "Failed to get PARTUUID on $bootdev, please partition and format /dev/$devname" && exit bootmountfile=$rootpartition/etc/systemd/system/boot.mount if [ -f $bootmountfile ] && grep -q '^What=UUID=' $bootmountfile; then echo setting PARTUUID for boot partition $bootdev ... mkdir -p $rootpartition/boot sudo chmod 666 $bootmountfile sudo sed -i s/What=UUID=.*/What=UUID=$uuid_boot/ $bootmountfile sudo chmod 644 $bootmountfile fi fi fstabfile=$rootpartition/etc/fstab if [ -f $fstabfile ] && ! grep -q '^/dev/root' $fstabfile; then sudo chmod 666 $fstabfile sudo echo "/dev/root / ext4 errors=remount-ro 0 1" >> $fstabfile sudo chmod 644 $fstabfile fi if [ -f $rootpartition/etc/apt/apt.conf ] && grep -iq 'acquire::http::proxy' $rootpartition/etc/apt/apt.conf; then sudo sed -i '/::proxy/d' $rootpartition/etc/apt/apt.conf fi fi if [ "$enable_efi" = y ]; then # configure grub.cfg for UEFI if [ -f $bootpartition/grub/${machine}_grub.cfg ]; then partuuid_boot=`lsblk -l --output PARTUUID $bootdev | grep -` partuuid_root=`lsblk -l --output PARTUUID $rootdev | grep -` sudo touch $bootpartition/$partuuid_boot sudo sed -i -e "s/partuuid_boot/$partuuid_boot/" -e "s/partuuid_root/$partuuid_root/" $bootpartition/grub/${machine}_grub.cfg if [ "$enable_acpi" = "y" ]; then sudo sed -i "s/console=.*,115200/acpi=force/g" $bootpartition/grub/${machine}_grub.cfg fi fi if ! mount | grep ${devpartname}$efipartnum; then sudo mount $efidev $efipartition fi sudo mkdir -p $efipartition/EFI/BOOT if [ -f $bootpartition/grub/${machine}_grub.cfg ]; then sudo cp $bootpartition/grub/${machine}_grub.cfg $efipartition/EFI/BOOT/grub.cfg fi if [ -f $bootpartition/grub/BOOTAA64.EFI ]; then sudo cp $bootpartition/grub/BOOTAA64.EFI $efipartition/EFI/BOOT/ fi if grep -q U-Boot $rootpartition/etc/buildinfo; then sudo sed -i '3d' $rootpartition/etc/buildinfo fi fi if [ $instruction = auto -o -n "$bootimg" -o -n "$rootfsimg" ]; then if [ -f $bootmountfile ] && ! grep -q $uuid_boot $bootmountfile; then print_e "Installation failed" else print_n "Installation completed successfully" fi fi if [ $bootpartnum != 2 -o $rootpartnum != 4 ] && [ `uname -m` = aarch64 ]; then print_w "NOTICE: as you configured non-default root and boot partitions, please reboot the board and in U-Boot run:" print_w "'setenv devpart_boot $bootpartnum;setenv devpart_root $rootpartnum;boot' to boot distro from the custom partition" fi } check_directory() { if [ -z "$force_install" -a ${devname:0:4} != loop ] && [ "`ls -A $1`" != "" -a "`ls -A $1`" != "lost+found" ]; then print_w "\nNOTICE: Appears $1 contains the existing data" read -t 180 -n 1 -p "Are you sure to drop the data in $1 partition to proceed now? [y/n] " rdresult && echo "" [ -z "$rdresult" ] && rdresult=n [ "$rdresult" != y -a "$rdresult" != n ] && echo $rdresult is invalid, valid: y or n && exit if [ $rdresult = n ]; then print_w "\nPlease backup important data in $1 if needed, or force the installation with '-F' option" && exit else echo Cleaning data in $1 && sudo rm -rf $1/* fi fi } check_running_rfs() { if mount | grep -q "$1 on / type ext4"; then print_w "Warnning: Can't install rootfs to the running root filesystem" print_w "Please select a non-running partition for the installation" && exit fi } check_distro_in_disk() { if [ -b $backupdev ] && ! mount | grep -q $backuppartition; then sudo mount $backupdev $backuppartition || true fi if [ -b $rootdev ] && ! mount | grep -q $rootpartition; then sudo mount $rootdev $rootpartition || true fi for tdir in $backuppartition $rootpartition; do if [ -d $tdir/var/lib ]; then check_directory $tdir fi done } check_images_format() { if [ -d $bootimg_n ]; then bootimgtype=dir elif file -L $bootimg_n | grep -q 'gzip compressed'; then bootimgtype=tgz elif file -L $bootimg_n | grep -q 'UUID='; then bootimgtype=ext elif [ $instruction != auto ] && [ -n "$bootimg" ] && [ ! -f $bootimg ]; then print_e "Not found $bootimg"; exit else bootimgtype=unknown fi if [ -d $rootfsimg_n ]; then rfsimgtype=dir elif echo $rootfsimg_n | grep -q .cpio.gz && file -L $rootfsimg_n | grep -q 'gzip compressed'; then rfsimgtype=cpio.gz elif file -L $rootfsimg_n | grep -q 'gzip compressed'; then rfsimgtype=tgz elif file -L $rootfsimg_n | grep -q 'UUID='; then rfsimgtype=ext elif [ $instruction != auto ] && [ -n "$rootfsimg" ] && [ ! -f $rootfsimg ]; then print_e "Not found $rootfsimg"; exit else rfsimgtype=unknown fi } check_network_access() { if echo $url | grep -q //; then remoteserver=$(echo $url | cut -d/ -f3) else remoteserver=$(echo $url | cut -d/ -f1) fi retcode=$(curl -I -m 10 -o /dev/null -s -w %{http_code} $remoteserver) || true if [ ${retcode:0:1} != 2 -a ${retcode:0:1} != 3 ]; then print_e "ERROR: HTTP returned $retcode, unable to access $remoteserver to fetch distro image" print_e "Please check your network to ensure $remoteserver is accessable via HTTP from this machine" print_e "Please check HTTP proxy settings if needed in your environment" exit fi } check_http_request() { retcode=$(curl -I -m 10 -o /dev/null -s -w %{http_code} $1) || true if [ "$retcode" != 200 -a "$retcode" != 000 ]; then print_e "The requested URL $1 returned error $retcode" exit fi } download_distro() { check_http_request $bootimg_url if [ -n "$machine" ]; then if [ -f ${firmware_url##*/} ]; then echo -e "${firmware_url##*/} already exists" elif [ $instruction = download ] || [ "$machine" != ls2088ardb -a "$machine" != ls1012ardb -a \ "$machine" != ls1012afrwy -a "$enable_efi" != y ]; then echo -e "\n Downloading $firmware_url ..." && curl -ROfk $firmware_url; [ $? != 0 ] && print_w "Not found $firmware_url" || ls -l ${firmware_url##*/} fi fi if [ -f ${bootimg_url##*/} ]; then echo -e "${bootimg_url##*/} already exists" else echo -e "\n Downloading $bootimg_url ..." && curl -ROfk $bootimg_url fi if [ -f ${rootfsimg_url##*/} ]; then echo -e "${rootfsimg_url##*/} already exists" else echo -e "\n Downloading $rootfsimg_url ..." && curl -ROfk $rootfsimg_url fi [ $? != 0 ] && print_e "Failed to download distro images" && exit print_n "Downloaded distro images [Done]" } print_e() { echo -e "${RED}$1 ${NC}" } print_n() { echo -e "${green}$1 ${NC}" } print_w() { echo -e "${YELLOW}$1 ${NC}" } print_d() { echo -e "${GREEN}$1 [Done] ${NC}" } RED='\e[1;31m' GREEN='\e[1;32m' green='\e[0;32m' YELLOW='\e[1;33m' NC='\e[0m' [ -z "$1" -o "$1" = "-h" -o "$1" = "--help" ] && usage && exit ARGS=$(getopt -a -o m:f:b:B:r:R:u:p:d:s:i:e:hvF \ -l machine:,firmware:,bootimg:,bootpart:,rootfsimg:,rootpart:,partition:,url:,device:,efi:,startblock:,instruction:,help,version,force -- "$@") [ $? -ne 0 ] && usage eval set -- "${ARGS}" while true do case "$1" in -m|--machine) machine=$2; shift;; -f|--firmware) firmware=$2; shift;; -s|--startblock) startblock=$2; shift;; -b|--bootimg) bootimg=$2; shift;; -B|--bootpart) bootpartnum=$2; shift;; -r|--rootfsimg) rootfsimg=$2; shift;; -R|--rootpart) rootpartnum=$2; shift;; -p|--partition) diskpartlist=$2; shift;; -u|--url) url=$2; shift;; -d|--device) mediadevice=$2; shift;; -i|instruction) if [ ${2:0:5} = auto: ]; then distrover=$(echo $2 | cut -d: -f2) echo distroversion: $distrover elif [ ${2:0:3} = pf: ]; then distrotype=$(echo $2 | cut -d: -f2) elif [ ${2:0:7} = backup: ]; then backupdir=$(echo $2 | cut -d: -f2) fi instruction=$(echo $2 | cut -d: -f1) shift;; -e|--efi) enable_efi=y echo "'-e' option is enabled for UEFI instead of U-Boot" [ "$2" = dtb ] && echo dtb is used for UEFI [ "$2" = acpi ] && enable_acpi=y && echo ACPI is enabled shift;; -v|--version) echo flex-installer version: $FIVERSION; exit;; -h|--help) usage;; -F|--force) force_install=y;; --) shift; break;; esac shift done if [ -n "$instruction" ] && [ $instruction != auto -a $instruction != pf -a $instruction != download \ -a $instruction != install -a $instruction != list -a $instruction != mksdcard -a $instruction != backup ]; then print_e "Invalid instruction $instruction, valid: auto, pf, download, install, list, mksdcard, backup"; exit fi default_machine_list='ls1012ardb ls1012afrwy ls1021atwr ls1028ardb ls1043ardb ls1046ardb ls1046afrwy ls1088ardb_pb ls2088ardb lx2160ardb_rev2 lx2162aqds ' if [ "$instruction" = list ]; then print_n "\nSupported machine list:" print_n " $default_machine_list" print_n "\nSupported invironment of installation:" print_n " Linux host PC, ARM board running LSDK distro, ARM board running TinyLinux"; exit fi [ -z "$distrotype" ] && distrotype=linux [ -z "$instruction" ] && instruction=null if [ -z "$mediadevice" ] && [ $instruction != download -a $instruction != mksdcard ]; then print_e "Please specify '-d '"; exit fi [ -f /etc/issue ] && [[ `cat /etc/issue | grep NXP | grep tiny` ]] && intinyrfs=y || intinyrfs=n [ $instruction = mksdcard -a -z "$mediadevice" ] && mediadevice=`sudo losetup -f` if [ $intinyrfs = y -a $instruction != download ]; then get_device_name_in_tinydistro elif [ $intinyrfs = n -a $instruction != download ]; then [ ! -b $mediadevice ] && print_e "$mediadevice does not exist on this host machine" && exit get_device_name_on_host fi default_linux_version=5.4 if [ $instruction = auto -o $instruction = pf ]; then disksize=$[ `sudo fdisk -ls /dev/$devname` / 1000000 ] print_n "/dev/$devname: $disksize GB" fi [ -z "$disksize" ] && disksize=0 [ -n "$distrover" ] && distroversion=$distrover || distroversion=${DEFAULT_DISTRO_SVR_URL##*/} if [ -z "$diskpartlist" ]; then [ "${devname:0:4}" = loop -o $disksize -le 8 ] && diskpartition=$DEFAULT_LOOP_DEVICE_PARTITION || \ diskpartition=$DEFAULT_DISK_PARTITION [ $instruction = auto -o $instruction = pf ] && [ $disksize -le 8 ] && \ print_w "The capacity of /dev/$devname is only $disksize GB, using partitions: $DEFAULT_LOOP_DEVICE_PARTITION" else diskpartition=$diskpartlist fi check_partition_number if [ $pnum -le 4 ]; then [ -z "$rootpartnum" ] && rootpartnum=$pnum backuppartnum=$[ $pnum - 1 ]; else [ -z "$rootpartnum" ] && rootpartnum=$[ $pnum + 1 ] backuppartnum=$pnum; fi [ -z "$bootpartnum" ] && bootpartnum=2 efipartnum=1; if [ $instruction = auto -o $instruction = download ]; then if [ -z "$machine" ] || ! echo "$default_machine_list" | grep -q "$machine "; then print_w "Please specify correct '-m '" print_n "Valid machine name: $default_machine_list"; exit fi fi mntdir=/mnt bootdev=/dev/${devpartname}$bootpartnum rootdev=/dev/${devpartname}$rootpartnum backupdev=/dev/${devpartname}$backuppartnum bootpartition=$mntdir/${devpartname}${bootpartnum} rootpartition=$mntdir/${devpartname}${rootpartnum} backuppartition=$mntdir/${devpartname}${backuppartnum} [ -n "$efipartnum" ] && efidev=/dev/${devpartname}$efipartnum && efipartition=$mntdir/${devpartname}${efipartnum} [ "${machine:0:7}" = "ls1021a" ] && tgtarch=arm32 || tgtarch=arm64 [ -f $rootpartition ] && [ "`ls -A $rootpartition`" != "" ] && print_e "Directory $mntdir is not empty, please clean it first" && exit for i in $bootpartition $rootpartition $backuppartition $efipartition; do sudo mkdir -p $i done [ -n "$bootimg" ] && bootimg_n=$bootimg || bootimg_n=bootpartition_LS_${tgtarch}_lts_${default_linux_version}.tgz [ -n "$rootfsimg" ] && rootfsimg_n=$rootfsimg || rootfsimg_n=rootfs_${distroversion}_ubuntu_main_${tgtarch}.tgz [ -n "$firmware" ] && firmware_n=$firmware || firmware_n=firmware_${machine}_uboot_sdboot.img [ "$machine" = ls2088ardb -a -z "$firmware" ] && firmware_n=firmware_${machine}_uboot_norboot.img [ "${machine:0:7}" = ls1012a -a -z "$firmware" ] && firmware_n=firmware_${machine}_uboot_qspiboot.img if [ -z "$url" -a -z "$distrover" ]; then url=$DEFAULT_DISTRO_SVR_URL elif [ -z "$url" -a -n "$distrover" ]; then url=${DEFAULT_DISTRO_SVR_URL%/*}/$distrover fi bootimg_url=$url/$bootimg_n rootfsimg_url=$url/$rootfsimg_n firmware_url=$url/$firmware_n [ ! -f /usr/bin/curl ] && [ $instruction = auto -o $instruction = download ] && \ print_e "not found curl, please install curl package" && exit for pkg in parted curl sudo fuser mount mkfs.ext4; do if ! which $pkg 1>/dev/null 2>&1; then print_w "Not found $pkg command, please install it first!"; exit fi done if [ $instruction = auto ]; then check_device_partitions check_network_access [ $intinyrfs = y ] && cd $rootpartition download_distro check_images_format flex_install_distro elif [ $instruction = pf ]; then partition_format_disk $diskpartition elif [ $instruction = download ]; then check_network_access download_distro elif [ $instruction = install -o $instruction = null ] && \ [ -n "$bootimg" -o -n "$rootfsimg" -o -n "$firmware" ]; then if [ "$enable_efi" = y ] && [ -z "$machine" ]; then print_e "Please specify '-m ' for UEFI installation"; exit fi check_device_partitions check_images_format flex_install_distro elif [ $instruction = mksdcard ]; then if mount | grep $mntdir/$devname; then sudo umount $mntdir/$devname* 1>/dev/null 2>&1 || true; fi [ ! -f $rootfsimg_n ] && print_e "Not found $rootfsimg_n" && exit [ ! -f $firmware_n ] && print_e "Not found $firmware_n" && exit print_n "Creating sdcard.img, waiting ..." rm -f sdcard.img && dd if=/dev/zero of=sdcard.img bs=1M count=$DEFAULT_SDCARD_IMG_SIZE_MB loopdev=$(sudo losetup -j sdcard.img | cut -d' ' -f1) if [ -n "$loopdev" ]; then for lpn in $loopdev; do sudo losetup -d ${lpn::-1} done fi sudo losetup /dev/$devname sdcard.img [ -n "$bootimg" ] && bootimgopt="-b $bootimg_n" [ -n "$diskpartition" ] && diskpartitionopt="-p $diskpartition" flex-installer -i install -r $rootfsimg_n -f $firmware_n $bootimgopt $diskpartitionopt -d /dev/$devname sudo losetup -d /dev/$devname fdisk -l sdcard.img elif [ $instruction = backup ]; then mount_device [ -z "$backupdir" ] && backupdir=$backuppartition; mkdir -p $backupdir; timestamp=$(date +%Y%m%d%H%M) cd $bootpartition && print_n "Backup $backupdir/backup_bootpartition_$timestamp.tgz ..." sudo tar czf $backupdir/backup_bootpartition_$timestamp.tgz * cd $rootpartition && print_n "Backup $backupdir/backup_rootfs_$timestamp.tgz ..." sudo tar czf $backupdir/backup_rootfs_$timestamp.tgz * ls -l $backupdir/backup*.tgz print_n "Backup completed successfully" else print_e "Incorrect usage, run 'flex-installer -h' to see help info" fi