DCB

Define constant byte.

[ label] DCBarg[,arg,...,arg]

Remarks

The DCB directive allocates and initializes a byte of memory for each arg argument. The arg may be a byte integer constant, a single- or multiple-character string constant, a symbol, or a byte expression. The DCB directive may have one or more arguments separated by commas. Multiple arguments are stored in successive byte locations. If multiple arguments are present, one or more of them can be null (two adjacent commas), in which case the corresponding byte location is filled with zeros.

If label is present, it is assigned the value of the runtime location counter at the start of the directive processing.

Integer arguments are stored as is, but must be byte values (e.g. within the range 0-255); floating-point numbers are not allowed. Single- and multiple-character strings are handled in the following manner:

Example

TABLE DCB 'two',0,'strings',0

CHARS DCB 'A','B','C','D'

See also

BSC

DC