An expression may be either relative or absolute. An absolute expression is one which consists only of absolute terms.
A relative expression consists of a relative mode. All address expressions must adhere to these definitions for absolute or relative expressions. This is because only these types of expressions retain a meaningful value after program relocation.