The Ethernet TAP probe provides troubleshooting utilities that let you test communications dynamically, without making any permanent changes to the flash EPROM of the Ethernet TAP probe. Any settings will be lost after the Ethernet TAP probe is reset.
Use the host command to edit the host table by assigning hostnames to specific IP addresses without permanently storing the changes in the Ethernet TAP probe flash EPROM. When entered without options, the host command displays the current host table. See netparam (netparamadd_host) to permanently store an address in flash.
host add hostname ip_address
The system adds the specified hostname to the host table.
host delete hostname ip_address
The system removes the specified hostname from the host table.
Hostnames are also cleared from the host table after the Ethernet TAP probe is reset.