Ethernet TAP probe setup utility commands and variables

The following is a list of all the Ethernet TAP probe internal setup utility commands. They are explained in greater detail, and grouped by functionality in the pages that follow.

Functionality Command Description
Configuration and Operational Commands netparam Sets non-volatile networking parameters.
tgtty Sets the target system serial port settings.
floader Enables the flash loader program.
logout Exits the internal setup utility.
reset Reboots the Ethernet TAP probe.
who Displays open user connections.
Troubleshoot Communications Commands arp Displays the ARP table commands.
host Displays the host table commands.
netstat Displays network statistics.
ping Tests if host is connected to your network.
route Sets dynamic network routing.
Utility Commands alias Manages aliases for commonly used commands.
batch Downloads and executes a command file.
history Displays command history list.
Advanced Troubleshooting Commands di Displays all the environment variables.
lsas Prints shell application assertions.
set Sets an environment variable.
unset Removes an environment variable.
Built-in Environment Variables Commands batchfile File containing commands to execute at boot.
batchpath Default location to search for batch files.
env_protect Prevents changes to settings in flash.
username Defines a username which must be entered when logging in using telnet.