ColdFire BDM connector information

The CodeWarrior Ethernet TAP ColdFire BDM probe has a 26-pin connector which automatically supports target system signal levels from 1.8V to 3.3V.

The following figure shows the pin assignments of the probe BDM connector.

Figure 1. Ethernet TAP probe ColdFire BDM connector pin assignments
Ethernet TAP Probe ColdFire BDM Connector Pin Assignments

The following table lists BDM signal names, direction, pin numbers, descriptions, and drive capabilities of the probe BDM connector.

Table 1. Ethernet TAP probe ColdFire BDM signal directions
BDM pin Signal mnemonic Signal direction Description
1 Reserved From target system 17pF load
2 BKPT From Ethernet TAP probe connector 50mA driver
3 GND - n/a -  
4 DSCLK From Ethernet TAP probe connector 50mA driver
5 GND - n/a -  
6 Reserved Bi-directional Open-drain, 100Ohm to ground when asserted by Ethernet TAP probe, 22pF load when not asserted
7 RESET Bi-directional Open-drain. 100Ohm to ground when asserted by Ethernet TAP probe, 22pF load when not asserted1
8 DSI From Ethernet TAP probe connector 50mA driver
9 VDD From target system 2MOhm pull-down, plus 0.01uF load
10 DSO From target system 17pF load
11 GND - n/a -  
12 PST3 - n/a -  
13 PST2 - n/a -  
14 PST1 - n/a -  
15 PST0 - n/a -  
16 DDATA3 - n/a -  
17 DDATA2 - n/a -  
18 DDATA1 - n/a -  
19 DDATA0 - n/a -  
20 GND - n/a -  
21 Reserved - n/a -  
22 Reserved - n/a -  
23 GND - n/a -  
24 PSTCLK From target system 17pF load
25 Core Voltage - n/a -  
26 TEA From Ethernet TAP probe connector 50mA driver1

The table below provides a general description of each BDM signal and operational requirements.

Note: All ColdFire BDM signals must meet accepted standards for ColdFire BDM signal design. To ensure proper and stable operation between the Ethernet TAP probe and the target system, the BDM signals must meet the requirements listed in the following table.
Table 2. Ethernet TAP probe ColdFire BDM signal recommendations and requirements
BDM pin Signal mnemonic Requirement
1 Reserved Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
2 BKPT Must be wired to the target system.
3 GND Must be wired to the target system. GND is connected directly to the ground inside the Ethernet TAP probe.
4 DSCLK DSCLK must be connected to the target system's processor. It is driven by the Ethernet TAP probe as an output with up to 50mA. This signal is the clock for the BDM interface. It is good design practice to keep the trace length short and isolate the trace from other signals. If the trace must be long, then termination may be needed.
5 GND Must be wired to the target system. GND is connected directly to the ground inside the Ethernet TAP probe.
6 Reserved Need not be wired to the target system. The Ethernet TAP does not currently use this signal.
7 RESET Must be wired to the target system. During reset, the Ethernet TAP probe drives RESET to ground through a 100Ohm resistor.
8 DSI Must be wired to the target system processor. The Ethernet TAP probe drives the DSI output with up to 50mA.
9 VDD Must be wired to the target system. The Ethernet TAP probe uses this signal to determine if power is applied to the target system. The signal is also used as a voltage reference for the signals driven by the Ethernet TAP probe (BKPT, DSCLK, RESET, DSI, and TEA).
10 DSO Must be wired to the target system processor. It is an input to the Ethernet TAP probe.
11 GND Must be wired to the target system. GND is connected directly to the ground inside the Ethernet TAP probe.
12 PST3 Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
13 PST2 Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
14 PST1 Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
15 PST0 Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
16 DDATA3 Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
17 DDATA2 Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
18 DDATA1 Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
19 DDATA0 Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
20 GND Must be wired to the target system. GND is connected directly the ground inside the Ethernet TAP probe.
21 Reserved Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
22 Reserved Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
23 GND Must be wired to the target system. GND is connected directly to the ground inside the Ethernet TAP probe.
24 PSTCLK Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
25 Core Voltage Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
26 TEA Need not be wired to the target system. The Ethernet TAP probe does not currently use this signal.
1 4.7Ohm pull-up to buffered TGT PWR.