Microsoft provides support for TCP/IP protocol with Windows. If your host PC does not already have TCP/IP protocol installed, you need to add it.
If you are installing a second Ethernet adapter to dedicate to the Ethernet TAP probe, you need to install a second instance of TCP/IP. In both instances, you bind the adapter to the TCP/IP protocol stack.
To install and configure TCP/IP, you need:
If you want other users to have access to the Ethernet TAP probe over the network, do not use the instructions in this section. Instead, see Connecting to network topic.
The Control Panel window appears.
The Network Connections window appears.
A context menu appears.
The properties dialog box appears.
The General page appears.
The Select Network Component Type dialog box appears.
The Select Network Protocol dialog box appears.
The Select Network Protocol dialog box closes.
The TCP/IP protocol is added to the host PC.
The Control Panel window appears.
The Network Connections window appears.
The context menu appears.
The network connection properties dialog box appears.
The General page of the properties dialog box appears.
The Internet Protocol (TCP/IP) Properties dialog box appears.
The IP address text boxes associated with this selected option appear.
If the PC is already on an existing network, assign the second adapter an IP and netmask inconsistent with your network topology (use Class C if LAN is Class B, for example). This allows the PC to easily resolve communication with the LAN versus the Ethernet TAP probe. Valid possible internal-use IP addresses for each class are:
| A | 10.0.0.0 - 10.255.255.255 | 255.0.0.0 |
| B | 172.16.0.0 - 172.31.255.255 | 255.255.0.0 |
| C | 192.168.0.0 - 192.168.255.255 | 255.255.255.0 |
If the PC is to remain standalone, use the address and netmask listed below. These addresses simplify configuration.
Address: 192.168.1.1
Subnet mask: 255.255.255.0
If not prompted, restart Windows manually.