You can use the Windows ping command to ensure that the Ethernet TAP probe can communicate with the host.
At the Windows command prompt, type the following:
ping hostname | ip_address
where hostname is the name and ip_address is the IP address assigned to the Ethernet TAP probe.
You should see screen output that indicates a reply from hostname that includes the IP address. If not, check the following: