As shipped, the Ethernet TAP probe acquires its network configuration automatically using DHCP. If necessary, you can manually enter a network configuration. If you cannot use DHCP, you must configure the probe for your network's address resolution protocol using static IP address resolution.
To manually configure the network settings of the Ethernet TAP probe for your network requirements, connect a terminal to the probe configuration port (Config Serial) and use the probe on-board setup utility (netparam) to change probe network settings. The probe netparam utility lets you select and modify network parameters that are saved in probe memory. Use netparam to configure the probe to match your network address resolution and routing protocols.
If the probe must be able to communicate with hosts on other subnets, you will need to configure the probe for one of the following routing options:
For more information, see Commands to configure communications and Network administration topics.
The core> command-line prompt appears.
To complete the steps presented in this section you need write permissions to the network database or the assistance of your network system administrator.
Example: Assign a static IP address and hostname to the Ethernet TAP Probe
If the Ethernet TAP probe has a static IP address of 195.121.1.2 and a hostname of lab01, enter the following commands:
core> netparam bootconfig static:lab01
core> netparam static_ip_address 195.121.1.2
core> reset
The netparam utility writes its settings into non-volatile memory on the probe. Follow these rules when using netparam: