Connecting probe tip to Ethernet TAP probe

To connect the probe tip:

  1. Verify that the Ethernet TAP probe is not connected to power.
  2. Connect the probe tip 50-pin D-style connector to the TARGET PROBE connector on the Ethernet TAP probe.
    Figure 1. Ethernet TAP probe with probe tip attached
    Ethernet TAP Probe with Probe Tip Attached

Instructions for connecting the Ethernet TAP probe to the target hardware are in Connecting to target system.