Connecting power supply cable

To connect the power supply cable:

  1. Install the plug for your environment onto the power supply.
    1. Depress the tab labeled `Push' on the back of the power supply.
    2. Slide the required connector into the slot.
      Figure 1. Install plug onto power supply
      Install Plug onto Power Supply
  2. Connect the power supply DC cable connector to the POWER connector on the Ethernet TAP probe.

    Connect only the provided power supply to the Ethernet TAP probe.

    CAUTION:
    Other power supplies may look similar, but can damage the probe if the supply specifications differ from the required specifications.
    Figure 2. Ethernet TAP probe with a power cable attached
    Ethernet TAP Probe with a Power Cable Attached