Locale-aware collating string comparison that ignores letter case.
#include <extras/extras_string.h> int stricoll(const char *s1, const char *s2);
s1
A pointer to a null-terminated character string.
s2
A pointer to a null-terminated character string.
This function compares each character at s1 and s2 using the collating sequence specified by the LC_COLLATE component of the current locale. This function returns one of these values:
This facility is not specified in the ISO/IEC standards. It is an EWL extension of the standard libraries.