ldiv()

Computes the long integer quotient and remainder.

  #include <stdlib.h>
  
  ldiv_t ldiv(long int numer, long int denom);    
Parameter

numer

The numerator.

denom

The denominator.

Remarks

The ldiv_t type is defined in div_t.h as typedef struct { long int quot, rem; } ldiv_t;

ldiv() divides denom into numer and returns the quotient and remainder as a ldiv_t type.

This facility is not specified in the ISO/IEC standards. It is an EWL extension of the standard libraries.