You can use the Message Settings (refer to the figure listed below) dialog box to map messages to a different message class.
Some buttons in the dialog box may be disabled. For example, if an option cannot be moved to an information message, the Move to: Information button is disabled. The following table lists the options available in the Message Settings dialog box:
| Button | Description |
|---|---|
| Move to: Disabled | Disables selected messages. The disabled messages will no longer be displayed. |
| Move to: Information | Changes selected messages to information messages. |
| Move to: Warning | Changes selected messages to warning messages. |
| Move to: Error | Changes selected messages to error messages. |
| Move to: Default | Changes selected messages to their default message types. |
| Reset All | Resets all messages to their default message types. |
| OK | Exits this dialog box and saves any changes. |
| Cancel | Exits this dialog box without accepting any changes. |
| Help | Displays online help about this dialog box. |
The following table lists and describes the tabs available in the dialog box for each message group:
| Message Group | Description |
|---|---|
| Disabled | Lists all disabled messages. That means that messages displayed in the tab page will not be displayed by the Assembler. |
| Information | Lists all information messages. Information messages informs about action taken by the Assembler. |
| Warning | Lists all warning messages. When such a message is generated, translation of the input file continues and an object file will be generated. |
| Error | Lists all error messages. When such a message is generated, translation of the input file continues, but no object file will be generated. |
| Fatal | Lists all fatal error messages. When such a message is generated, translation of the input file stops immediately. Fatal messages cannot be changed. They are only listed to call context help. |
Each message has its own character (`A' for Assembler message) followed by a 4- or 5-digit number. This number allows an easy search for the message on-line help.