Content Area

The Assembler displays logging information about the assembly session in the content area. This logging information consists of:

When a file is dropped into the assembly window content area, the Assembler either loads the corresponding file as a configuration file or the Assembler assembles the file. The Assembler loads the file as a configuration if the file has the *.ini extension. If the file does not end with the *.ini extension, the Assembler assembles the file using the current option settings.

All text in the assembler window content area can have context information consisting of two items:

File context information is available for all output lines where a filename is displayed. There are two ways to open the file specified in the file-context information in the editor specified in the editor configuration:

If the Assembler cannot open a file even though a context menu entry is present, then the editor configuration information is incorrect (refer to the Editor Setting Dialog Box section below).

The message number is available for any message output. There are three ways to open the corresponding entry in the help file: