There are different ways to specify the input file which must be assembled. During assembling of a source file, the options are set according to the configuration performed by the user in the different dialog boxes and according to the options specified on the command line.
Before starting to assemble a file, make sure you have associated a working directory with your assembler.