Compiler, Assembler, Linker, Decoder, Debugger, Librarian, or Maker
HIENVIRONMENT
ENVIRONMENT=<file>
<file>: filename with path specification, without spaces
This variable has to be specified on the system level. Normally the Assembler looks in the current directory for an environment file named default.env ( .hidefaults on UNIX). Using ENVIRONMENT (e.g., set in the autoexec.bat (DOS) or .cshrc (UNIX)), a different filename may be specified.
ENVIRONMENT=\Freescale\prog\global.env