-WOutFile: Create error listing file

Group

Messages

Scope

Assembly Unit

Syntax

-WOutFile(On|Off)

Arguments

None

Default

Error listing file is created.

Description

This option controls if a error listing file should be created at all. The error listing file contains a list of all messages and errors which are created during a assembly process. Since the text error feedback can now also be handled with pipes to the calling application, it is possible to obtain this feedback without an explicit file. The name of the listing file is controlled by the environment variable ERRORFILE: Filename specification error.

Example
  -WOutFileOn

  

The error file is created as specified with ERRORFILE.

  -WErrFileOff
  
  

No error file is created.

See also

Assembler options: