Output
Application
-F(h|2o|A2o|2|A2)
h: HIWARE object-file format; this is the default
2o: Compatible ELF/DWARF 2.0 object-file format
A2o: Compatible ELF/DWARF 2.0 absolute-file format
2: ELF/DWARF 2.0 object-file format
A2: ELF/DWARF 2.0 absolute-file format
-F2
Defines the format for the output file generated by the Assembler:
Note that the ELF/DWARF 2.0 file format has been updated in the current version of the Assembler. If you are using HI-WAVE version 5.2 (or an earlier version), -F2o or -FA2o must be used to generate the ELF/DWARF 2.0 object files which can be loaded in the debugger.
ASMOPTIONS=-F2