Output
Assembly unit
-Le
None
None
Switches on the generation of the listing file, but macro expansions are not present in the listing file. The listing file contains macro definition and invocation lines as well as expanded include files.
ASMOPTIONS=-Le
In the following example of assembly code, the cpChar macro accepts two parameters. The macro copies the value of the first parameter to the second one.
When the -Le option is specified, the assembly code in the following listing along with additional source code (Listing: Example source code from an included file) from the macro.inc file generates an assembly output listing file (Listing: Example assembler output listing):
XDEF Start MyData: SECTION char1: DS.B 1 char2: DS.B 1 INCLUDE "macro.inc" CodeSec: SECTION Start: cpChar char1, char2 NOP
cpChar: MACRO LDA \1 STA \2 ENDM
Abs. Rel. Loc Obj. code Source line ---- ---- ------ --------- ----------- 1 1 XDEF Start 2 2 MyData: SECTION 3 3 000000 char1: DS.B 1 4 4 000001 char2: DS.B 1 5 5 INCLUDE "macro.inc" 6 1i cpChar: MACRO 7 2i LDA \1 8 3i STA \2 9 4i ENDM 10 6 CodeSec: SECTION 11 7 Start: 12 8 cpChar char1, char2 15 9 000006 9D NOP
The Assembler stores the content of included files in the listing file. The Assembler also stores the macro definition and invocation in the listing file.
The Assembler does not store the macro expansion lines in the listing file.
For a detailed description of the listing file, see the Assembler Listing File chapter.
-Lc: No Macro call in listing file