Output
Assembly unit
-L[=<dest>]
<dest>: the name of the listing file to be generated.
It may contain special modifiers (see Using Special Modifiers).
No generated listing file
Switches on the generation of the listing file. If dest is not specified, the listing file will have the same name as the source file, but with extension *.lst. The listing file contains macro definition, invocation, and expansion lines as well as expanded include files.
ASMOPTIONS=-L
In the following example of assembly code, the cpChar macro accepts two parameters. The macro copies the value of the first parameter to the second one.
When the -L option is specified, the portion of assembly source code in the following listing, together with the code from an include file ( Listing: Example source code from an include file) generates the output listing in Listing: Assembly output listing.
XDEF Start MyData: SECTION char1: DS.B 1 char2: DS.B 1 INCLUDE "macro.inc" CodeSec: SECTION Start: cpChar char1, char2 NOP
cpChar: MACRO LDA \1 STA \2 ENDM
Abs. Rel. Loc Obj. code Source line ---- ---- ------ --------- ----------- 1 1 XDEF Start 2 2 MyData: SECTION 3 3 000000 char1: DS.B 1 4 4 000001 char2: DS.B 1 5 5 INCLUDE "macro.inc" 6 1i cpChar: MACRO 7 2i LDA \1 8 3i STA \2 9 4i ENDM 10 6 CodeSec: SECTION 11 7 Start: 12 8 cpChar char1, char2 13 2m 000000 C6 xxxx + LDA char1 14 3m 000003 C7 xxxx + STA char2 15 9 000006 9D NOP
The Assembler stores the content of included files in the listing file. The Assembler also stores macro definitions, invocations, and expansions in the listing file.
For a detailed description of the listing file, see the Assembler Listing File chapter.
Assembler options: