Host
None
-LicBorrow<feature>[;<version>]:<Date>
<feature>: the feature name to be borrowed (e.g., HI100100).
<version>: optional version of the feature to be borrowed (e.g., 3.000).
<date>: date with optional time until when the feature shall be borrowed (e.g., 15-Mar-2005:18:35).
None
None
None
This option lets you borrow a license feature until a given date/time. Borrowing allows you to use a floating license even if disconnected from the floating license server.
You need to specify the feature name and the date until you want to borrow the feature. If the feature you want to borrow is a feature belonging to the tool where you use this option, then you do not need to specify the version of the feature (because the tool is aware of the version). However, if you want to borrow any feature, you need to specify the feature's version number.
You can check the status of currently borrowed features in the tool's About box.
-LicBorrowHI100100;3.000:12-Mar-2005:18:25
Assembler options: