The Save Configuration tab of the Configuration dialog box contains all options for the save operation. The following image displays the Save Configuration tab of the Configuration dialog box.
In the Save Configuration tab, you can select which items to save into a project file when the configuration is saved.
This dialog box has the following configurations:
Almost all settings are stored in the project configuration file. The only exceptions are: