The example in the following listing shows a typical layout of the configuration file (usually project.ini).
[Editor] Editor_Name=IDF Editor_Exe=c:\Freescale\prog\idf.exe Editor_Opts=%f -g%l,%c [HC08_Assembler] StatusbarEnabled=1 ToolbarEnabled=1 WindowPos=0,1,-1,-1,-1,-1,390,107,1103,643 WindowFont=-16,500,0,Courier TipFilePos=0 ShowTipOfDay=1 Options=-w1 EditorType=3 RecentCommandLine0=fibo.asm -w2 RecentCommandLine1=fibo.asm CurrentCommandLine=fibo.asm -w2 EditorDDEClientName=[open(%f)] EditorDDETopicName=system EditorDDEServiceName=msdev EditorCommandLine=c:\Freescale\prog\idf.exe %f -g%l,%c