0/1/2/3/4
This entry specifies which editor configuration is active:
- 0: global editor configuration (in the file
mcutools.ini)
- 1: local editor configuration (the one in this file)
- 2: command line editor configuration, entry EditorCommandLine
- 3: DDE editor configuration, entries beginning with EditorDDE
- 4: CodeWarrior with COM. There are no additional entries.
For details, see also
Editor Setting Dialog Box.
Only with
Editor Configuration set in the
File > Configuration > Save Configuration dialog box.