Complex application or application involving several programmers can be split into several simple modules. In order to avoid any problem when merging the different modules, the following rules must be followed.
For each assembly source file, one include file must be created containing the definition of the symbols exported from this module. For the symbols referring to code label, a small description of the interface is required.