Example of a PRM file (Test2.prm)

Listing: Separating assembly code into modules-Test2.prm

LINK test2.abs /* Name of the executable file generated. */
NAMES

  test1.o

  test2.o / *Name of the object files building the application. */

END

SECTIONS

  MY_ROM  = READ_ONLY  0x2B00 TO 0x2BFF; /* READ_ONLY  mem. */

  MY_RAM  = READ_WRITE 0x2800 TO 0x28FF; /* READ_WRITE mem. */

END

PLACEMENT

  /* variables are allocated in MY_RAM          */

  DataSec, DEFAULT_RAM           INTO MY_RAM;

  /* code and constants are allocated in MY_ROM */

  CodeSec, ConstSec, DEFAULT_ROM INTO MY_ROM;

END

INIT  entry      /* Definition of the application entry point. */

VECTOR ADDRESS 0xFFFE entry /* Definition of the reset vector. */
Note: The CodeSec section is defined in both object files. In test1.o, the CodeSec section contains the symbol AddSource. In test2.o, the CodeSec section contains the entry symbol. According to the order in which the object files are listed in the NAMES block, the function AddSource is allocated first and the entry symbol is allocated next to it.