Source line

This column contains the source statement. This is a copy of the source line from the source module. For lines resulting from a macro expansion, the source line is the expanded line, where parameter substitution has been done. See the following listing:

Listing: Example listing file - Source line column

 Abs. Rel.   Loc    Obj. code   
Source line


 ---- ----   ------ ---------   -----------

    1    1                      
;-------------------------------



    2    2                      
; File: test.o



    3    3                      
;-------------------------------



    4    4

    5    5                               
XDEF  Start



    6    6                      
MyData: SECTION



    7    7   000000             
char1:  DS.B  1



    8    8   000001             
char2:  DS.B  1



    9    9                               
INCLUDE "macro.inc"



   10    1i                     
cpChar: MACRO



   11    2i                                
LDA   \1



   12    3i                                
STA   \2



   13    4i                              
ENDM



   14   10                      
CodeSec: SECTION



   15   11                      
Start:



   16   12                               
cpChar char1, char2



   17    2m  000000 C6 xxxx    +           
LDA char1



   18    3m  000003 C7 xxxx    +           
STA char2



   19   13   000006 9D                   
NOP



   20   14   000007 9D                   
NOP