Obj. code

This column contains the hexadecimal code of each instruction in hexadecimal format. This code is not identical to the code stored in the object file. The letter ` x' is displayed at the position where the address of an external or relocatable label is expected. Code at any position when ` x' is written will be determined at link time. See the following listing:

Listing: Example listing file - Obj. code column

 Abs. Rel.   Loc    
Obj. code

   Source line
 ---- ----   ------ ---------    -----------

    1    1                      ;-------------------------------

    2    2                      ; File: test.o

    3    3                      ;-------------------------------

    4    4

    5    5                               XDEF Start

    6    6                      MyData:  SECTION

    7    7   000000             char1:   DS.B  1

    8    8   000001             char2:   DS.B  1

    9    9                               INCLUDE "macro.inc"

   10    1i                     cpChar:  MACRO

   11    2i                                LDA   \1

   12    3i                                STA   \2

   13    4i                              ENDM

   14   10                      CodeSec: SECTION

   15   11                      Start:

   16   12                               cpChar char1, char2

   17    2m  000000 
C6 xxxx

    +          LDA char1

   18    3m  000003 
C7 xxxx

    +          STA char2

   19    13  000006 
9D

                   NOP

   20    14  000007 
9D

                   NOP