RAD50 - RAD50-encoded string constants

Syntax
RAD50 <str>[, cnt]
Synonym
None
Description

This directive places strings encoded with the RAD50 encoding into constants. The RAD50 encoding places 3 string characters out of a reduced character set into 2 bytes. It therefore saves memory when comparing it with a plain ASCII representation. It also has some drawbacks, however. Only 40 different character values are supported, and the strings have to be decoded before they can be used. This decoding does include some computations including divisions (not just shifts) and is therefore rather expensive.

The encoding takes three bytes and looks them up in a string table. The following listing shows the RAD50 encoding.

Listing: RAD50 Encoding

unsigned short LookUpPos(char x) {
  static const char translate[]=

    " ABCDEFGHIJKLMNOPQRSTUVWXYZ$.?0123456789";

  const char* pos= strchr(translate, x);

  if (pos == NULL) { EncodingError(); return 0; }

  return pos-translate;

}

unsigned short Encode(char a, char b, char c) {

  return LookUpPos(a)*40*40 + LookUpPos(b)*40

                            + LookUpPos(c);

}

If the remaining string is shorter than 3 bytes, it is filled with spaces (which correspond to the RAD50 character 0).

The optional argument cnt can be used to explicitly state how many 16-bit values should be written. If the string is shorter than 3*cnt, then it is filled with spaces.

See the example C code below about how to decode it.

Example

The string data in the following listing assembles to the following data where 11 characters are contained in eight bytes. The 11 characters in the string are represented by 8 bytes.

Listing: RAD50 Example

  XDEF rad50, rad50Len
DataSection   SECTION

rad50:        RAD50 "Hello World"

rad50Len:     EQU (*-rad50)/2
Listing: Assembler output where 11 characters are contained in eight bytes

$32D4 $4D58 $922A $4BA0

This C code shown in the following listing takes the data and prints "Hello World".

Listing: Example-Program that Prints Hello World

#include "stdio.h"
extern unsigned short rad50[];

extern int rad50Len; /* address is value. Exported asm label */

#define rad50len ((int) &rad50Len)

void printRadChar(char ch) {

  static const char translate[]=

    " ABCDEFGHIJKLMNOPQRSTUVWXYZ$.?0123456789";

  char asciiChar= translate[ch];

  (void)putchar(asciiChar);

}

void PrintHallo(void) {

  unsigned char values= rad50len;

  unsigned char i;

  for (i=0; i < values; i++) {

    unsigned short val= rad50[i];

    printRadChar(val / (40 * 40));

    printRadChar((val / 40) % 40);

    printRadChar(val % 40);

  }

}