PAGE
None
Insert a page break in the assembly listing.
The portion of code in the following listing demonstrates the use of a page break in the assembler output listing.
code: SECTION DC.B $00,$12 DC.B $00,$34 PAGE DC.B $00,$56 DC.B $00,$78
The effect of the PAGE directive can be seen in the following listing.
Abs. Rel. Loc Obj. code Source line ---- ---- ------ --------- ----------- 1 1 code: SECTION 2 2 000000 0012 DC.B $00,$12 3 3 000002 0034 DC.B $00,$34 Abs. Rel. Loc Obj. code Source line ---- ---- ------ --------- ----------- 5 5 000004 0056 DC.B $00,$56 6 6 000006 0078 DC.B $00,$78