END
None
The END directive indicates the end of the source code. Subsequent source statements in this file are ignored. The END directive in included files skips only subsequent source statements in this include file. The assembly continues in the including file in a regular way.
The END statement in the following listing causes any source code after the END statement to be ignored, as in the next listing.
Label: DC.W $1234 DC.W $5678 END DC.W $90AB ; no code generated DC.W $CDEF ; no code generated
Abs. Rel. Loc Obj. code Source line ---- ---- ------ --------- ----------- 1 1 000000 1234 Label: DC.W $1234 2 2 000002 5678 DC.W $5678