The operand is addressed then the HX register is incremented.
This addressing mode is useful for searches in tables. It is only used with the CBEQ instruction. See the following listing for an example of an example of using the indexed with post-increment addressing mode.
XDEF Entry ORG $F000 data: DC.B 1,11,21,31,$C0,12 CodeSCT: SECTION Entry: LDHX #$00FF TXS main: LDA #$C0 LDHX #data LOOP: CBEQ X+,IS_EQUAL BRA LOOP IS_EQUAL: ...
Using this addressing mode, it is possible to scan the memory to find a location containing a specific value.
The value located at the memory location pointed to by HX is compared to the value in the A register. If the two values match, the program branches to IS_EQUAL. HX points to the memory location next to the one containing the searched value.
In this example, the value $C0 is searched starting at memory location $F000. This value is found at the memory location $F004, the program branches to IS_EQUAL, and the HX register contains $F005.