The View menu lets you customize the Assembler window. You can specify if the status bar or the toolbar must be displayed or be hidden. You can also define the font used in the window or clear the window. The following table lists the View menu options.
| Menu Entry | Description |
|---|---|
| Toolbar | Switches display from the toolbar in the Assembler window. |
| Status Bar | Switches display from the status bar in the Assembler window. |
| Log... | Customizes the output in the Assembler window content area. The following two entries in this table are available when you select Log: |
| Change Font | Opens a standard font dialog box. The options selected in the font dialog box are applied to the Assembler window content area. |
| Clear Log | Clears the Assembler window content area. |