Message/Error Feedback

After assembly, there are several ways to check where different errors or warnings have been detected. The default format of the error message is as shown in the following listing.

Listing: Typical error feedback message
Default configuration of an error message
>> <FileName>, line <line number>, col <column number>, 

pos <absolute position in file>

<Portion of code generating the problem>

<message class><message number>: <Message string>

A typical error message is like the one in the following listing.

Listing: Error message example
>> in "C:\Freescale\demo\fiboerr.asm", line 18, col 0, pos 722
         DC    label

              ^

ERROR A1104: Undeclared user defined symbol: label

For different message formats, see the following Assembler options: