Line Number can be Specified on the Command Line

Editors like UltraEdit-32 or WinEdit (v95 or higher) can be started with a line number in the command line. When these editors have been correctly configured, they can be started automatically by double clicking on an error message. The configured editor will be started, the file where the error occurs is automatically opened and the cursor is placed on the line where the error was detected.