Editor Started with DDE

Enter the service, topic and client name to be used for a Dynamic Data Exchange (DDE) connection to the editor (refer to the figure listed below). All entries can have modifiers for the filename and line number, as explained in the Modifiers section.

Figure 1. DDE Editor Configuration
DDE Editor Configuration

For the Microsoft Developer Studio, use the settings in the following listing:

Listing: Microsoft Developer Studio configuration settings
Service Name: msdev
Topic Name:   system

Client Command: [open(%f)]