Assembling a File which has Already been Assembled

The commands executed previously can be displayed using the arrow on the right side of the command line. A command is selected by clicking on it. It appears in the command line. The specified file will be processed when the button Assemble in the toolbar is selected.