RS08 Assembler > Language

Use this panel to specify code- and symbol-generation options for the RS08 assembler.

The following image shows the Language panel.

Figure 1. Tool Settings - RS08 Assembler > Language
Tool Settings - RS08 Assembler > Language

The following table lists and describes the language options for RS08 Assembler.

Table 1. Tool Settings - RS08 Assembler > Language Options
Option Description
Angle brackets for macro arguments grouping (-CMacAngBrack) Controls whether the < > syntax for macro invocation argument grouping is available. When it is disabled, the Assembler does not recognize the special meaning for < in the macro invocation context. There are cases where the angle brackets are ambiguous. In new code, use the [? ?] syntax instead. Options are:
  • Allow
  • Disallow
Square braces for macro arguments grouping (-CMacBrackets) Controls the availability of the [? ?] syntax for macro invocation argument grouping. When it is disabled, the Assembler does not recognize the special meaning for [?] in the macro invocation context. Options are:
  • -CMacBracketsON
  • -CMacBracketsOFF
Maximum MacroNest nesting (-MacroNest) Controls how deep macros calls can be nested. Its main purpose is to avoid endless recursive macro invocations.