Use this panel to specify the host settings of the RS08 assembler.
The following image shows the Host settings.
The following table lists and describes the memory model options for RS08.
| Option | Description |
|---|---|
| Set environment variable (-Env) | This option sets an environment variable. Use this environment variable in the maker, or use to overwrite system environment variables. |
| Borrow license feature (-LicBorrow) | This option allows you to borrow a license feature until a given date or time. Borrowing allows you to use a floating license even if disconnected from the floating license server. |
| Wait until a license is available from floating license server (-LicWait) | By default, if a license is not available from the floating license server, then the application will immediately return. With, -LicWait set, the application will wait (blocking) until a license is available from the floating license server. |
| Application Standard Occurrence | This option allows you to select the standard appearance for the application window. By default the option -ViewHidden is selected. For more Information, refer to the section -View: Application standard occurrence. |